Other Parts Discussed in Thread: OPA4376, LM7705
请教各位大侠:
最近在使用OPA4376做一个项目,需要对一个几十uV级的直流信号进行放大,在使用OPA4376时遇到了一些问题。
问题1:单电源5V供电,当输入V+ 和V-均接地时,输出1端有100mV的电压输出,请问是什么原因引起的?
问题2:当V-接地,V+输入一个50mV的电压时(该电压是通过1M、10K电阻对5V分压后输出到V+端),输出1端输出1V(放大20倍),结果正确;
但当V+输入一5mV的电压时(该电压是通过1M、1K电阻对5V分压后输出到V+端),输出1端输出电压144mV,为什么不是100mV?
电路如下: