这么设计合理吗,如果分压电阻提高到2M呢?如果不合理应该如何改动,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,单位跟随的话,
1)补偿电容100nF可以不需要的。
2)输出接二极管上拉到3.3V,也去掉。
3)驱动容性负载的的输出隔离电阻R175可以适当小一些,一般是22ohm~100ohm之间。 您使用100ohm应该问题也不大,可以使用TINA仿真试试。
可以去掉,考虑到实际运放都会有输入偏置电流的影子,那么会和这个电阻形成压降。
这样会由于运放两个输入端的电阻不同,引起的偏移也不同,那么可能会由于正负输入端的偏移差异作为额外误差。
如果源阻抗有50ohm或者100ohm阻抗的话,可以在反馈回路上加上,这样会消除由于两个输入端的偏移造成的误差。