This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在使用PGA308做设计,请教此芯片的电压基准问题

Other Parts Discussed in Thread: PGA308, PGA309, INA129

如题,在使用PGA308做设计,pga308输出不稳,电压输出飘达10mV,在烤箱中做的实验,30,40,50,60度恒温条件下测试的,这样的输出现在是不能接受的,现在的ref是和芯片的供电脚和外接传感器的供电脚接一起的,芯片的寄存器配置和Vref是有关的,由于Vref的微小变化,是否会影响输出?如何改善?

  • 您好,

    您的这个问题,不是PGA308的问题。

    1,PGA308是不带温度补偿的,如果您需要做温度补偿,可以选用PGA309。

    2,“现在的ref是和芯片的供电脚和外接传感器的供电脚接一起的”

    您这样接法是不争取的,     不能跟外接传感器的供电接到一起。因为做补偿的过程中,是需要动态调整传感器的激励电压的。

  • 谢谢,昨天做个新实验,发现有一个问题,PGA308刚上电到稳定输出会有2分钟左右的时间,这期间输出会有4mV左右的涨幅,经过很多片实验,这期间都是往上涨的,而且数值上有会4mV左右。而我们旧的设计使用的是INA129,这期间只有1mV左右的涨幅,我想问的是,是PGA308本身的特性,还是我电路的问题?

  • 工作稳定之后,pga308表现得很好,那这期间的涨幅,是正常的吗