Other Parts Discussed in Thread: LM358
LM358接成电压跟随器时,同相输入端悬空,输出高电平。此特性何解?
还有哪些运放有这种特性?
请推荐,用在放大uV级,1-200HZ信号上。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM358
LM358接成电压跟随器时,同相输入端悬空,输出高电平。此特性何解?
还有哪些运放有这种特性?
请推荐,用在放大uV级,1-200HZ信号上。
我最近用358也遇到这么个问题,我当时将输入端与地短接,然后就直接变0了,我当时想的是可能是失调的原因
老师你好,我现在有信号的输入,358跟随器与前端是通过一个104的瓷片电容耦合的,但是这样一个信号过来后,358是跟随器,但是最后的现象是358输出有一个直流偏置,但是这个偏置是慢慢的从0向上升的,我怎么去解决这个问题?,在输入端加一个合适的电阻嘛?望解答,谢谢
你测一下输出电压,然后除以增益,看看与358的失调是否相近?有可能是失调影响。
另:如果交流信号,为什么不在输出端也接一个电容再耦合给后级电路呢?
如果输入阻抗很小,运放的同相端偏置电流将会对输入电容充电,特别是当输入信号变化缓慢的时候。这种情况下,会在开机后一段时间内产生输出直流偏置。在输入电容后面挂一个连接到地的电阻可以减少这种效应,但同时也损失了输入阻抗。
我需要做单边带的调制,所以那个直流我“舍一得扔”,我是仅仅做了一个跟随器,如果前一级与358直接耦合的话,就没有那个现象,一切正常,我就在358的输入那加了一个1M的电阻,然后用了一个470的电解电容耦合的,现在正常了