This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OP27和OP37搭建的放大電路振盪



 昨天搭建出這個電路后,剛開始沒加10uF的電容,只有0.1uF的退耦電容後來加上2.2uF后,注意到從20K到400K左右的頻段內出現振盪,由正弦到方波再到很不正常的波形大於400多K之後又正常了,有點巧了?呵呵(這個電路我感興趣的頻段是1K到200K,這是個局部圖,這部份調試是獨立的)。今天早上再次測試發現全頻段都可以放大了,只是正弦波信號質量不高,零輸入,出來的信號有個一二十毫伏的干擾,尖峰現象嚴重,很亂,調節示波器觀察那一段波形有點像過沖后的振鈴現象,一段一段的。感覺是出於臨街振盪,這個頻段有幾M吧,不知道該怎麼解決這種問題了。

在這裡說明一下,前端信號輸入為1K到200K的DDS信號輸出,300mV左右的直流偏置,在1K時峰峰值600左右,200K的時候只有二三十mV了。我想先“均衡”一下再放大。