Other Parts Discussed in Thread: OPA2365, OPA227
如图所示是一个运放的开环增益曲线。根据相位裕量的定义:增益为0dBm时,相移与180的差值,则从图中可以估计出该运放的相位裕量不到22°。并且,该测试曲线是在CL=0pF时,测得的曲线。
1、这是否说明,该运放实际使用时,是一定有一定量的过冲?
2、如果在该运放输出端加一个RC低通滤波器,是不是相当于添加了一个极点,导致相位裕量减少,从而可能引发震荡?
3、如果问题2答案是肯定的话,是不是说即使该运放的输入信号是直流的,也会出现震荡?(因为运放的稳定性与输入信号无关?)
4、如果问题3的答案是否定的话,那运放是会在什么频率的输入信号下出现震荡?
5、这样的运放(OPA2365)在RF=0.1RG时的反向比例放大器时,能稳定工作么?
6、同一个运放在同样的工作条件下,为何小信号时出现明显的过冲,但大信号时,过冲却不明显,见图片1和2?
望专家就以上6个问题一一详细解答,感激不尽!!!