Other Parts Discussed in Thread: OPA172, OPA192, LM124, LM2902, LM2902-N, LM124-N, OPA188
LM2902D的放大精度为多少?我想采用高精度电阻(精度:万分之五)配置LM2902D的放大倍数,放大倍数误差范围是多少?
有没有其他精密运放推荐?电源有+12V、-12V、+5V、-5V供电,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
lm124和LM2902精度差不多,属于通用运放,精度属于一般的标准,可以使用LM124-N或者LM2902-N
LM124资料上没有LM124-N的型号啊?有这个型号么?
LM124-N是高精度的么?
如果收入电压为0到30V,LM124-N供电电压应为多少?
有这个型号,你在官网搜索LM124-N或者直接点击LM124-N即可找到,输入电压0-30V的话建议使用30-32V供电
LM124-N的精度是多少?
如上面的电路图所示,如果输入电压0到30V超过了供电电压12V,会损坏运放吗?
供电电压只影响运放输出电压吧?
谢谢!
精度相关的参数(Vos/VOS Drift/Ios/IOS Drift/etc.)可以查看数据手册得到,如果输入电压0-30V超过了供电电压12V不会损坏该运放,供电电压影响运放输出电压,是对的
官方的DATASHEET里面有LM124J的封装,LM124-N也是DIP的么?
是的,LM124-N也是DIP封装的,事实上,LM124J和LM124-N指的同一款器件,LM124-N的Orderable Device 名称就是LM124J。
请问是什么应用?您所谓的高精度主要是针对交流特性还是直流特性?请描述一下具体应用,我们根据您的应用为您推荐合适的运放。另外如果您想要达到一个比较高的精度,光从运放着手,有时候可能并不能解决问题,要从系统端入手,在ADC以及基准源的选择上都要求高精度。所以还是要根据您的应用要求来选型。谢谢!
OPA188,OPA192都有不错的直流特性,可以参考一下,并且OPA192的输入输出均为轨至轨, 采用e-trim技术将直流参数做了校准。另外不知道您对ADC有没有高精度的需求,对于直流信号采样,TI有多款16/24 bit delta-sigma ADC供选择,配合REF50XX系列低温漂基准源,可以从系统级提高精度要求。
需要高精度ADC采样?有没有好的芯片和具体的电路推荐?谢谢!