Other Parts Discussed in Thread: PGA309, XTR117
关于PGA309有几个问题请教一下专家:
1、假如进行线性补偿,需要用到引脚1--VEXC,这个引脚的最大激励电流是5mA吗?如果不是5mA这个有没有具体的一个值?这个激励电流的大小是否和可以提供给PGA309芯片的供电电流有关系?假设给传感器供电的电源最大可以提供的电流为4mA,那这激励电流能达到5mA吗?
2、 在使用XTR117+PGA309的电路中,查询XTR117的VREG引脚可以提供的输出电流为3.8mA,而PGA309的不带负载时需要消耗的电流最大为1.6mA,而且VREG还给24LC16BE供电,查询24LC16BE可以查到ICC WRITE 的电流为最大3mA,ICC READ的电路为最大1mA,如果以最大电流计算的话两个芯片的供电电流已经超过了3.8mA,请问问题出现在什么地方了,这个供电电流的关系应该怎么计算啊?