Other Parts Discussed in Thread: OPA659
输入信号:约0.2mV左右的,脉冲宽度100ns的脉冲信号。信号频率:10KHz。想请教一下对于这样的脉冲信号,运放的带宽定为多少合适。我目前还没确定信号带宽多少合适,打算按照40M左右进行设计.
运放选择opa659.采用两级串联,形成中放。采用反向比例运算电路。即输入信号接反向端。我看了器件的手册。上面对输入信号有要求。Common-Mode Input Range
TA = –40°C to +85°C ±2.87 ±3.37 V B。就是对于输入信号的共模电压范围最小值为2.87V,典型值为3.37V。我想请教的是,对于放大我的输入信号,是否意味着需要加入最小为2.87V的直流偏置电压,作为芯片的直流工作点电压。那么我想问的是,按照反向比例放大的电路。该直流偏置电压如何加?
即放大器的正向输入端,原本接GND。如果要加直流偏置电压的话,是否为偏置电压Vref=2.87,串接一电阻(其值为Rg并Rf),然后接正向输入端?是否如此?
那么对于放大器的反向输入端,直流偏置电压如何加?
我的电话:15984682450(谢工)