Part Number: INA146
VIN+正常情况下输入信号是-10~10V,VIN-=-10V,我希望把这个信号变成0~3V后送入F28335 AD口;在我没有接外界输入;在我没有接外界信号的时候,就是VIN+不接,VIN-=-10V,输出Vo是多少?Vo是多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
FIGURE 1电路如下截图所示,A1运放实现的是将差分输入衰减10倍,即VOA1= (VIN – VIN) 0.1
A2是同向比例放大电路,增益是1 + RG2/RG1
正常情况下当实现
输入信号是-10~10V,VIN-=-10V,我希望把这个信号变成0~3V
这个功能时,A2运放的增益需是1.5倍,即如下电路(我这里A2同向和反向输入端没有做阻抗匹配)

当VIN+不接悬空时,A1运放相当于反向比例放大电路,增益是-0.1,A2运放的功能不变,因此VIN-=-10V输入时,A1输出是1V,A2输出是1.5V