This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用OPA2695芯片搭建的三级运放,输出的幅频特性上面有出现周期性的上跳,求原因

电路原理图如下

有三级放大电路,第一级同相输入,第二、第三级反相输入。三级输出的频响是这样的:

这个是从1MHz到100MHz的幅频响应曲线,看到在50MHz的时候出现了一个上跳的现象。不仅在50MHz上面会出现这种现象,而是在100MHz、150MHz、200MHz上面都会周期地出现,增益越大越明显。这个上跳不是因为反馈电阻取小而导致的,实际测试的时候发现面有50MHz的信号通过正负电源线耦合进电路里。在绘制PCB电路的时候,两块芯片是采用一点接电源的方式,而在两块芯片的电源线之间接有一个LC滤波,示意图如下:

但是无论如何调整电感的值,都没办法消除电源线上面存在的交流信号。PCB电路的电源部分如图:

P1、P2、P3分别是用插针接入的正负电源以及地。想请问一下,那个存在于电源线中的50MHz交流信号是不是因为,PCB电源部分布局布线过于冗杂产生了类似分布电容引起的,还是电路本身产生的电磁辐射,亦或是其他原因,谢谢了。