Other Parts Discussed in Thread: OPA388, OPA387, TLV376
目的是利用OPA847做一个脉冲信号(100mV,脉宽200ns,频率5K,)的放大电路,电路图已贴上,由于没有负电源,想用5V直流单电源。
调试结果是没输出,TP1处电压是0.12V左右,TP2处电压2.7V,无信号。
硬件菜鸟,请问各位老师,如何更改,如何调试呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,首先OPA847的供电电压典型值为+-5V,最大+-6V,那么单电源供电的话也是10V·12V之间。所以您使用单电源5V是不可以的。
其次就是它不是轨至轨输入,通过datasheet中的电气参数可以看到,+-5V供电时,同相反相输入端的电压典型值为+-3V。也就是说和电压轨有2V左右的headroom。
因此单电源供电的话,最低输入大概也在2V左右。所以给100mV输入是不满足其线性工作电压范围的。
OPA847是一款高增益带宽(3.9Ghz)的运放,您的信号频率并不大,所以如果单电源供电,可以考虑选择其他运放。
您的要求是100mV,脉宽200ns,频率5K输入,输出需要多大幅值,或者说需要增益多大?
很多运放都可以实现,首先单电源供电,因为输入幅值比较小,所以尽量选取轨至轨输入,其次就是带宽要够,因为信号带宽较低,所以大多数运放的带宽都是够用的。我选了几款精度运放比如OPA387,OPA388,TLV376等。我使用OPA387简单的仿真了下,假如0~1V输入,Gain=3输出0~3V,仿真如下:
更多运放可以参考下面选型链接进行筛选:
下面结果是我根据rail to rail input,单通道,带宽筛选出来的一些器件,您也可以比较下。