求麦克风的前置放大电路与带通滤波电路?另外这两者连接还需不需要驱动电路呢???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPA3112 这个器件的性能很好的. 不过从手册看, 输入端有个阻抗匹配方面的要求. 要留意一下
Gain setting via GAIN0 and GAIN1 inputs
The gain of the TPA3112D1 is set by two input terminals, GAIN0 and GAIN1. The voltage slew rate of these gain terminals, along with terminals 1 and 14, must be restricted to no more than 10V/ms. For higher slew rates, use a 100kΩ resistor in series with the terminals.
The gains listed in Table 1 are realized by changing the taps on the input resistors inside the amplifier. This causes the input impedance (ZI ) to be dependent on the gain setting. The actual gain settings are controlled by ratios of resistors, so the gain variation from part-to-part is small. However, the input impedance from part-to-part at the same gain may shift by ±20% due to shifts in the actual resistance of the input resistors.
For design purposes, the input network (discussed in the next section) should be designed assuming an input impedance of 7.2 kΩ, which is the absolute minimum input impedance of the TPA3112D1. At the lower gain settings, the input impedance could increase as high as 72 kΩ
你好,
TPA3112是模拟输入音频功率放大芯片,在你的应用中是麦克风输出信号直接送到功率放大级对吗?
如果是这样是没有问题的,需要注意麦克风输出是单端还是差分,与TPA31112之间采用交流耦合。
对于TPA3112来说,SD pin与Fault直接连接是为了在输出短路解除时从shut down状态自动恢复。