上一小节,简单介绍了几个基于REF200的高精度电流源的方案。它们的共同特点就是电路简单,温漂小。但设计都是几组固定值,如果我们想要一个任意值的电流源,该如何设计呢?这一小节主要介绍使用REF200来实现任意值的电流源的方法。
我们先试想一下,如果我们有100uA的电流源,那怎样设计出任意值的电流源呢,如220uA,47uA? 好像是个问题。不过我们可以沿着这个思路来实现这个设计,我们有100uA的电流源,理论上就可以设计出M*100uA电流源。这个M可以是整数也可以是小数。这个比例可以用不同的电阻实现。如下图所示
通过调整R1和R2的关系就可以实现(N+1)*100uA的电流源。这个电路的基本原理利用运放的跟随原理。来保证两个电阻上的电压值是相等的,则流过电阻的电流之比,就是两个电阻的反比。这个电路,对运放的输出驱动能力,输入偏置电流和失调电压要求都比较高。因此像TI的OPA602是比较合适的。同样的两个电阻也需要高精度(0.1%),低温漂的电阻。
如果需要比100uA小的电流源呢,可以实使用下面的电路来实现。它的输出Iout=N*100uA.
如下表,选用不同的电阻比例,就可以实现不同的电流源。同样的这个设计对运放和电阻都有同上一个设计的要求。推荐高精度的运放OPA602或OPA128等都不错。