This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家帮忙推荐一款5MHz以上、输入阻抗1G以上的运放,谢谢
有没有电源、输出电流等条件?可以先看看OPA141/OPA2141/OPA4141
Hi Carter,
谢谢你.
我是想做一个传感器滤波放大的输入级电路。传感器电容10pF~200pF,信号为100kHz~5MHz。因此要达到100kHz的高通滤波效果,输入级至少需要1/2pifc=160k欧姆的阻抗。为保险起见我想把输入阻抗设定为1M欧,之前看到一个运放CA3130,15MHz Zi=1.5T欧 Ii=5pA,但是高频的时候就不行了。因此可能所需要的频率更高一些才行,这个OPA141我大概仿真了一下,输出很奇怪 您看一下:
我是用TINA-TI仿真是没有问题的哦,请看图:
原来是我设置的仿真初始条件是0点,仿真时间不够,可以频率还是不够用
把分压电阻换成4.5V电源是一样的