Other Parts Discussed in Thread: LM339
工程师你好,
我在阅读LM339规格书时,看到有如下图的描述:
请问该怎么理解?如果供电5v,接地0v,那么上图是否表征IN+与IN-的差值不得超过(5-1.5)V?
如果该差值超过3.5V ,会有什么风险呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,这里指的输入共模电压范围是0~(VCC-1.5V).比如5V单电源供电,那么IN+和IN-的输入电压范围为0~3.5V。
VCC-2这里的限制是比较保守的,考虑到温度的影响,比如5V供电,0~3V是最安全的。
如果不满足这个输入共模电压范围的话,比较器将不会线性工作,功能受到影响。
项目中我需要比较两个5V的电平(均为数字开关量),按照这样的话,我觉得有两种解决思路:
1.提升比较器电源,VCC最少需要6.5V,例如接入12V电源,此时输入高电平依旧为5V,满足(VCC-1.5)的要求
2.设定比较器电源为5V,然后降低输入的两个信号电平,使用1%精度电阻对两个输入电平进行1/2分压。此时输入高电平为2.5V,也满足(VCC-1.5)的要求。
请问这两种方案是否都OK呢?
您好,这两种方案都是可以的,主要满足其输入共模电压范围内即可保证比较器的正常工作。
另外注意LM339是open drain输出,比较器输出高电平取决于上拉电压Vlogic,所以12V电源供电,如果需要比较器高电平输出5V, 需要上拉Vlogic=5V。
感谢答疑,
另外还有一个问题,我看比较器规格书中没有关于输出最大容性负载的要求,是否意味着输出可以使用一阶RC进行滤波(R大约在100到1000欧姆之间,C大约为0.01到0.1uF之间)?
您好,输出加RC滤波,R作为和容性负载的隔离电阻一般是没问题的,但是LM339的数据手册中虽然没有给出最大容性负载值,给出了测试条件基本上是在15pF的条件下测试的,所以我用TINA仿真了下,0.1uF和100ohm 的仿真如下:可以看到输出有失真
CL改为15pF之后,输出基本正常。