想问下一种运算放大器,输入在5v以内,能放大到10v输出
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
有其他参数要求吗?比如说通道数、输入失调电压、带宽、压摆率、输出电流能力、输出范围等?如果没有其他要求的话,看下 LM358BA,因为它是满足您上述要求价格最便宜的产品,它最小输入电压可以到负电源轨,最大供电电压可以到36V。
在正负输入均为0-5v时候
您是要将两输入信号做差分运算吗?或者说您具体要实现什么样的功能?
如果您只是需要将5V的电压放大到10V,那么您不需要非得选择输入电压可以到负电源轨的运放,很多运放使用比例放大电路都可以满足要求,如下电路结构:
您可以看下 LM324B,我这次重新选型的时候发现上次选型参数选择可能有误,您可以忽略我上次的参数选型。
考虑到运放带载有输出电压降的情况,建议您使用12V或15V给LM324B供电。
5V的供电肯定实现不了10V的输出。若需要10V的输出,至少11V供电,具体取决于输出电流的大小。
之前有用LM358但是这个芯片到3v多就已经饱和。
这里您具体是怎样应用的?这里3V是指输入电压吗?供电电压几伏,5V吗?如果是5V供电,输入电压范围到3.5V左右,过高的输入电压会使输出饱和或截止,如下输入范围截图:
如上所述,运放输出10V至少需要10V以上的供电电压,因此若VCC=5V是不能输出10V的
是的,还是提醒您要注意LM124不是轨至轨输出,输出最大电压与输出电流有关,输出电流越大,最大输出电压降越大,这里建议您至少使用12V,甚至保险起见使用15V电压供电才能保证输出10V电压。
不客气~