This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2187: the output of OPA2187

Part Number: OPA2187

Hi 

I set up a Non-inverting amplifying circuit with OPA2187, the diagram showed as below picture. 

when I add the voltage into the Non-invertering input pin, there are some problems with the output voltage. for example, when add 0.5V into pin 5, the voltage of pin 7 will be 1V. But sometimes, the output voltage will become 1.024V. see the below first picture. When I changed R5 from 10K to 5.1K, this situation happened more often. see the below second picture.

I don't know why the output voltage sometimes become more than twice the input voltage.

Looking forward to your reply.

       

thanks and best regards

Kim