BUF602在缓冲DC信号时,VREF引脚如何连接?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,BUF602这颗缓冲器设计的就是为交流信号通过AC耦合到输入端,然后通过内部偏置电流将其偏置到1/2(V+-V2-)电压,减少外部偏置电路的搭建,使用起来非常方便。
看下内部电路,Vref输出1/2{(V+)-(V-)}。如果单电源5V供电,则Vref输出2.5V,同样如果双电源供电,则Vref等于零。
那没关于您提到的缓冲直流信号,其实和交流信号一样,如果您不需要抬升直流信号电压,则可不用它,如果比如-3V也想抬高电压,也可以将Vref接到输入端。
但如果缓冲直流信号,不需要Vef的话,也可以考虑使用其他缓冲器或者搭建单位跟随都可以。
Vref是输出1/2Vcc电压,不用的话可以直接悬空。
DC信号,怎么还有250Mhz的时钟?
还是我理解错了,您指的缓冲直流信号,不是指的BUF602输入DC 信号吗?
DC耦合的前提是输入电压要满足BUF602的输入电压要求。 比如+-2V的信号,假如单电源供电,则负压输入是不允许的,这时我们可以使用REF给输入信号加偏置使其提高到满足输入电压范围内。
如果双电源供电,比如+-5V供电,+-2V输入是没问题的,那么REF可直接悬空,下面是我用TINA对250Mhz,+-2V输入仿真结果,REF悬空: