Other Parts Discussed in Thread: OPA820, LMH6629, OPA695
原理图和PCB layout如下,留了一些空位用来debug,比如C14/C15/C20/C21板子上短路掉了。
目前VGA可以工作,但问题是添加反馈环路之后,积分器OPA820的输出一直饱和在4.3~4.4V之间,导致AGC并不能发挥作用。无论我设置OPA820的正输入端为多少,例如1 V,它的输出始终饱和;
1、想让该AGC放大70~100MHz的信号,如果短路C28,请问积分器中的C27/R17/R16分别取多少值合适?
2、在肖特基二极管之后,是否有必要接一个低通滤波器或并接一个电容来平滑曲线?R23/C24/R15分别取多少合适?
3、取Rf=1k,Rg=200,第一级VGA的放大在10MHz时倍数是正常的,但是到100MHz,会比10MHz时多放大很多倍。我之前做的其他高速运放(比如OPA695 / LMH6629)也出现了同样的问题,请问是因为什么导致的?电阻我是用的普通电阻,请问会不会是电阻频响的问题,在100MHz必须要用RF电阻?
谢谢!