Other Parts Discussed in Thread: LM833
各路大神帮帮忙,我的需求是这样的:
原始信号是200kHz的小信号,幅度大概是几mv或10几mv,想放大到3V以内的水平,但工作过程中会受到约40kHz左右的信号干扰,幅度可能到V级,即200kHz信号是叠加在40kHz信号之上的,我想采集和放大的是200kHz的那个小信号。用2级运放如何实现这一点呢?
另外,请问LM833使用单电源供电可以正常工作吗?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM833
各路大神帮帮忙,我的需求是这样的:
原始信号是200kHz的小信号,幅度大概是几mv或10几mv,想放大到3V以内的水平,但工作过程中会受到约40kHz左右的信号干扰,幅度可能到V级,即200kHz信号是叠加在40kHz信号之上的,我想采集和放大的是200kHz的那个小信号。用2级运放如何实现这一点呢?
另外,请问LM833使用单电源供电可以正常工作吗?谢谢!
1000 被左右的增益, 还有外加滤波器, 可以找 http://webench.ti.com/ 帮你吧
你好,
两级放大+带通滤波来实现.
请问这是一个什么应用?40kHz信号为何会这么大
Hi Mike,
You are so solid and professional ,why we use band pass filter not band rejection filter, thank you.
你好,
感谢您的回复,这是一个红外感光方面的应用,红外接收管(光电二极管)接收发射管的信号,发射管的开关频率大概是200kHz,每接收完对面若干个发射管信号(顺序开关)后,就切换到下一个接收管,依次类推,接收管的切换频率大概是40kHz左右,因为存在外界光干扰(比如阳光),相当于每个接收管都因为外界光干扰而存在一个基底信号了,而且此基底对于各接收管不尽相同,如果外界光比较强的话,这个基底就会比较高。我想让这个方案能够有比较好的抗光性。能大概给出一个参考电路么,谢谢!