Other Parts Discussed in Thread: OP07
1)功能描述:
4路OP07模拟量输入接口电路(4路的地是同一个模拟地,供电电源均采用同一路±12V模拟电源,4路在同一块PCB板上,并排挨在一起)。OP07做射随使用(-10~+10V直流电压射随,直流应用!),输入阻抗(输入端下拉电阻使用的是3M,确实有点大,但由于接口要求,输入阻抗不能太小,不然对接后信号会降低)。
2)现象:
4路输入,什么都不接,OP07输出大约是3~5mV,一直在跳动。(正常)
当其中1路接入信号(其余3路还是什么都不接),接入电压例如5V(由安捷伦电源提供),输出很稳定,数值几乎不跳动(4.997~4.998V),但其他3路跳动很大,跳动范围大约-5~50mV,有时出现100mV多的值;
此时,我将第二路接入一个电压,例如1V,输出就很稳定了,数值几乎不跳动(1.000~1.001V).
3)问题
不知道大家明白了没?就是我全部悬空输入(当然靠输入引脚的3M电阻拉地),输出有跳动,但最大10mV,可能是噪声电流引起的,属于正常;
为什么我其中一路接入信号后,其他3路悬空的,输出噪声竟然变成100mV多?无法理解??当我把跳动很大的路接入信号后,就很稳定了。
请高手帮我解答,模拟电路深似海,所以我要多多学习请教,请大侠们指教