This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AD623输出信号出现正选波动

Other Parts Discussed in Thread: REF3212, OPA2335

问题描述:小弟在用AD623做应变调理电路,电路如附件示意图中的图1所示,电路由锂电池供电。做好PCB板之后,用示波器发现AD623输出信号中有约50Hz的正选波动,其中还混杂有很多高频毛刺,如示意图中的图2所示。

我采用的方法和效果:经过检测所有器件都工作正常,我在输出端加上了一个截止频率为100Hz的4阶低通滤波器,可以很好的滤除高频毛刺,但对50Hz的正弦波动没有效果,且本电路要求有100Hz的带宽,所以不能再把滤波器的截止频带降低了。由于我是用锂电池供电的,所以对于50Hz的正弦波动,我怀疑是示波器引入的工频噪声;但又觉得不太可能,因为同样用示波器观察电路中REF3212的输出确实是1.25的直流。对正弦波动的由来很是疑惑!!!

请教:还请各位指教,这些正弦波动和高频毛刺产生的原因和避免的方法,谢谢!