在输入大于210mV时,输出出现错误,,,这是什么情况,该如何解决呢?Voverdrive是指我的输入电压吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,先看下您的电路,单电源5V供电,IN-接GND,信号源您这里应该是+-210mV是吗?因为如果0~210mV的话,经过比较之后输出恒为高电平。
所以通过波形来看,信号源应该是+-210mV,然后和IN-进行比较。
但是TLV3501的输入电压范围最低为(V-)-0.2V,所以单电源供电的话,最低不能低于-200mV。
所以我想您提到的“在输入大于210mV时,输出出现错误”。正相端大于210mV的同时,负压也低于-210mV,所以不在TLV3501的输入电压范围内了,因此也就不保证正常工作。
如果您改为双电源供电,就不会有问题了。