This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VCA810: 问题描述如下:

Part Number: VCA810
Other Parts Discussed in Thread: OPA192

VCA810供电电压±5V,输入信号200KHz的,幅值±1V的VPP,参数配置放大2陪,输出失真

1.原理图如下

2.波形图如下

其中通道2为输入信号(绿色),通道1为输出信号(黄色)

  • 从输出波形来看,Gain=3,并且相位超前,您说的失真是不是这个意思?

    是在靠近VCA810的输入输出端测试的吗?测试点T3前面输入加了低通滤波是吗?

    方便断开外围电路,只测试VCA810看下是否正常,电路里R18 是为了隔离C35吗? 因为C35 对于OPA192来说是容性负载,并且很大,会导致不稳定吗,如果想通过R18进行隔离,建议这里使用小阻值,22~100ohm范围内。