Other Parts Discussed in Thread: XTR112
你好
我使用了XTR112搭建了一个4~20mA的电流发送器,组建了一个PID智能控温仪。
目前向使用外接带有PT100温度传感器和半导体制冷器的红外探测器(HgCdTe)时,发现输出的4~20mA电流太小,无法满足应用需求。
请问,能不能通过电流放大的方式,在原来4~20mA电流输出的基础,将电流放大到0.2A到0.5A左右。
TI有没有相关的电流放大设计参考方案呢!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
采用三线制4-20mA的结构即可。
如果是驱动激光器需要使用大的可调电流源,可以考虑使用LED驱动电路实现,可以做到较高的效率,从而提高制冷的效率。