Other Parts Discussed in Thread: AMC1302
您好,我使用INA333作为压力传感器的前端信号调理电路。压力传感器的输出范围是0~12mV,传输距离十米左右。INA333的输出作为隔离运放AMC1302的输入,但是我发现整个电路的输出都不一致性太差,我做了10路同样的电路。请问这里需要这么改进?是不是INA333的输出需要进行电压跟随?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
其中信号的输入规格是4±△V,这样的设计可以检测到这个信号吗?
5V供电,输入共模是4V左右的话,输出电压是有限制的,请参见Figure 21. Typical Common-Mode Range vs Output Voltage,希望能满足您的需求。您可以先通过仿真软件验证您的设计。
datasheet:
https://www.ti.com/lit/ds/symlink/ina333.pdf#page=10
Simulation model:
https://www.ti.com.cn/product/cn/INA333#design-tools-simulation
是可以满足的。但是小电压会有问题,Output需要满足大于50mV. 请关注手册第5页参数Output voltage swing from rail
不矛盾,第一张图是输入对应到输出的配置。
第二幅图的意思时,当前条件,输出电压的范围时绿色线的范围,即4V共模的话,输出电压的范围是0.1~1.8V。
但是,这个并不全面,输出电压范围,并不能到达电源轨,还受到输出电流等因素的限制。