1、信号源是频率125khz、幅值20mv的信号。2、项目背景信号是通过ook调制的小信号,想把信号通过可增益放大器放大后,再经AD采样,进入dsp处理,dsp选用的是TI的6748.问下大家,放大器和AD选用哪款呢?谢谢哈。
补充:放大器用两级放大,前一级用100倍左右,第二级用20倍左右,第二级用可编程增益放大器;AD用14位的可以满足,三路的AD;信号是125khz的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
125K的信号,100倍的放大,如果希望对125K信号放大能保证高于1%的精度,那么放大器的带宽积将会是大于1GHz,这样的运放使用起来会比较麻烦点。
是否可以考虑三级,每级10倍,使用带宽积为几十兆左右的运放,会方便很多。
您好,谢谢您这几天耐心的帮我。刚看了下ADS7946的资料,采样率是2 MSPS,采样频率是满足125khz的输入信号,但我看datasheet的曲线图时,像图里的SINAD vs FREE-AIR TEMPERATURE图,它的fin是20khz,是不是ADS7946用的典型频率就是20khz呢?SINAD vs INPUT FREQUENCY这个曲线图的指标最大频率fin是100khz,我采样的频率是125khz,这样不要紧吧?还有ADS7946是个两通道的,能不能介绍个三通道,并口输出的呢?谢谢。
这个是12位的,不知道能否满足你的要求。一般情况下,选择ADC,位数,速度,供电,输入范围和通道数,输出接口是最基本的要求。然后就看DC 的参数,AC的参数是否满足要求。