Other Parts Discussed in Thread: INA129
1、问题概述:
电路使用单电源工作,仪放5脚输入2.5V参考电压,基于单电源实现压电陶瓷信号阻抗匹配及放大。常温环境下,电路正常工作,压电陶瓷产生的信号能被仪放正常放大;当温度上升至180℃时,压电陶瓷产生的信号无法正常放大,输出端几乎没有信号。电路测试过程中,压电陶瓷在室温环境下,其它电路在高温环境,所有阻容器件耐温200℃。
2、测试数据:
用万用表监测本电路中INA129的2、3脚之间电阻R(电路带电),测试结果如下:
常温 : R=10MΩ
140℃: R=9.4MΩ
160℃: R=6.7MΩ
180℃: R=0.8MΩ
3、问题总结
温度提高至180℃时,为什么输入阻抗会这么低,而手册里标注的输入阻抗数量级是10,请问是我用的不对吗,应该怎么处理?