Other Parts Discussed in Thread: INA333
INA333的手册中标识出静态电流是50uA,但动态功耗在手册中没有找到,或者是我没有理解。这个动态功耗是否有计算公式?例如和输入信号的差分幅度、放大器的增益倍数、供电电压等等的关系?
实际测试中,采用+2.5v和-2.5v供电,增益倍数设置为1000, 输入端无信号时(Vin+, Vin-悬空),输出基本在0电平,电流在0.5mA左右。如果在输入端引入工频干扰(例如用手单独触摸Vin+),输出端测试到50Hz的工频干扰,并且已经饱和,电源电流达到5.0mA左右。
因为我们的系统中用到较多的模拟通道,每个通道最大5.0mA电流情况下,整个系统的累计电流非常大。请问我上面测量到的5.0mA电流是否属于正常情况?如何才能降低此电流?
谢谢!