This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

sn65dsi85 mipi转lvds 问题



1、我现在初始化sn65dsi后,读取0XE5 寄存器,值一直为0x80。即CHA_SYNCH_ERR。不知道产生该原因是什么?列出了以下几点可能的原因:

    1、mipi信号hsync、vsync出错(修改这两个极性,依然报0x80)

     2、修改lvds 输出极性。修改寄存器0x18的几个DE、HS POLARITY、VS POLARITY报同样的错误。

     3、SYNC_DELAY出现了错误,寄存器0x28、0x29值没设对。

            Tuner配置里提到Line Time (SYNC to SYNC) Requirement (us),但是没看明白什么个意思。使用Tuner配置出来的参数 SYNC_DELAY_low一直为0x20。希望举个例子,解释下SYNC_DELAY是怎么计算出来的.

以下是lvds需要的参数,在mipi里也设置成了一样。不知道这样设置对不对?能否帮我设置个正确的配置?

mipi输出480M。
                lvds-format = <LVDS_8BIT_1>;
                out-face    = <OUT_P888>;
                
                clock-frequency = <85500000>;
                hactive = <1366>;
                vactive = <768>;
                
                hback-porch = <213>;
                hfront-porch = <70>;
                hsync-len = <143>;

                vback-porch = <24>;
                vfront-porch = <3>;                
                vsync-len = <3>;

               hsync-active = <0>;
                vsync-active = <0>;
                de-active = <0>;
                pixelclk-active = <0>;