This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

方波速率由16K提高到64K后,波形畸变

Other Parts Discussed in Thread: LM2902-N, TL084

我使用LM2902-N,正负5V供电,对3.3V的数字信号经过隔直后进行二阶低通滤波(1:1输出),前级也放了些RC构成无源低通滤波,

期望能将方波的高次谐波过滤得到近似正弦波

方波速率在原设计中是8K,当时也不太懂SR,这个芯片的带宽是1M,想着够用了,从实际结果看还是很理想

但是现在需求变了,速率提高到32K,就看到输出有很严重的畸变(尤其在变化沿),信号完全不可辨认

滤波器的参数已做相应更改,但结果是一样的,就是输出信号严重畸变

但是板子已不能更改,能否在现有的电路中做改进达到需求?