This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教DAC(DAC5682Z) 与IQ调制器(TRF370417)的接口问题

Other Parts Discussed in Thread: TRF370417, DAC5682Z, DAC5681

请教DAC(DAC5682Z) 与IQ调制器(TRF370417)的接口问题

一、    项目需求

项目需要利用DAC5682Z 与TRF370417产生所需调制的中频(IF)信号,文档SLAA399(Passive Terminations for Current Output DACs)给出了R2直流耦合时和电容C交流耦合是两种不同的连接方案。分别为文档的Figure12和Figure13所示。

二、针对Figure12和Figure13,设计者迷惑的地方,请予指导

在设计时时是否需要满足以下要求:

1、DAC5682Z的输出阻抗是否必须为50欧;

2、IQ调制器(TRF370417)的输入阻抗为5K欧姆,与DAC输出阻抗或者LC低通滤波器的输入输出阻抗相比较,是否可以看着为高阻。

3、DAC 输出 的I路或Q路 差分信号(I+和I-或Q+和Q-)的共模电压应该为3.3V;

4、IQ调制器(TRF370417)输入的I路或Q路 差分信号(I+和I-或Q+和Q-)的共模电压应该为1.7V;

5、有关LC 差分滤波器的设计可以参考参考SLWA053B文档(Design of Differential Filters for High-Speed Signal Chains)中单端LC滤波器变差分LC滤波器的方法与步骤,设计需要注意的地方就是LC差分滤波器的输入输出阻抗。

4、SLAA399文档Figure12中按照R1=72欧 ,R2=116欧,R3=124欧,R4=150欧的参数进行设计(R1,R2,R3,R4的参数遵从SLAA399文档P9页下部分的参数),此时LC滤波器的输入输出阻抗均为75欧(单端),由于直流电阻R2的存在使得接口电路对信号造成10.8dB的损耗。而在SLAA399文档Figure13中,按照R1= 127欧,R2=434欧,R3=462欧,R4=200欧进行设计(R1,R2,R3,R4的参数遵从SLAA399文档P10页上部分的参数),此时LC滤波器的输入输出阻抗均为100欧(单端),此时由于电容C对交流信号的旁路作用,那么接口电路对交流信号的损耗变为0dB。

综上所述,是否可以这样判定:LC滤波器输入输出阻抗是采用75欧姆(单端),还是采用100欧姆(单端)均可以,只要LC低通滤波器采用响应的阻抗匹配即可。

5、由于设计者项目中DAC产生的是宽带IQ基带信号(大于5MHz带宽),那么电容C的取值有何参考?是不是只需要小于1uF即可。(注:Typically, with values of C in the 1-uF range, the high-pass corner is approximately 100 Hz to 1 kHz.摘自 SLAA399  P8)。

三、在项目的设计过程中,设计者参考了DAC5682Z EVM(DAC5681/81z/82z EVM)文档,设计时存在以下疑问,请予指导。

1、从DAC5682Z EVM文档的P11页看出,DAC5682Z输出的IQ两路采用了5阶低通器进行滤波,低通滤波器的3dB带宽为300MHz左右。但是对DAC5682Z EVM的P42页的原理图分析

(1)如何判定原理图中是采用了5阶的低通滤波器?

(2)该低通滤波器的类型是什么(是Butterworth, Chebyshev, Cause ,Bessel,Tonne中的一种类型吗?)

(3)电阻R152,R154和R150的作用是什么

(4)原理图中滤波器的输入输出阻抗是多少

(5)DAC5682Z的输出阻抗是多少?

(6)电路中C105,C73,C116的作用是什么,标注为DNI,什么情况下才焊接。

(7)原理图中LC滤波器的负载电阻是哪个?与SLAA399文档中Figure12或Figure13中的R4能否对应得上?

(8)切了保证I路和Q路的幅相位一致性以及差分信号的通道一致性,DAC5682Z EVM的P42页的原理图中LC低通滤波器中电感L和电容 C的精度有什么要求?

  • 阻抗往往是得到最佳信号的条件.

  • 谢谢Airwill赐教。

        关于文档SLAA399  Figure13中,既要满足阻抗条件,又要满足共模电压偏置条件,按照图中的参数进行选取,共模电压得不到规定的3.3v和1.7v。按照R1= 127欧,R2=434欧,R3=462欧,R4=200欧进行设计(R1,R2,R3,R4的参数遵从SLAA399文档P10页上部分所列举的参数),3.3V和1.7V的共模电压的如何得到呢?以下计算方法正确吗?(计算见附件)