This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

常见高精度运放的噪音都有多大?(转载,欢迎坛友补充最新元器件)

Other Parts Discussed in Thread: OP07, OP27, OPA27, OPA227

运放是用途非常广泛的放大器,而所谓高精度运放,就是说其失调电压Vos小。 
运放的噪音,一律都是折算成输入端的值,这样才好计算、才好做对比。因此,若运放组成的放大器放大了100被,那么噪音也要×100。 
运放的噪音,一律都是用uVpp来表示而不是用rms来表示,大概是因为uVpp比较容易在示波器上观察出来。 

OP07是老一代经典运放,Vos=30uV、Ib=1nA,噪音uVpp=0.35uV,这成为后续运放的追求目标。事实上,电阻法7转10,如果没有更好的运放,用OP07也很不错。 
OP27是后续改进的运放,Vos=10uV、Ib=10nA,噪音uVpp=0.08uV。可以看到,Vos很小、噪音非常小,只不过Ib比较大了,不能用在7转10电路上 
AD707B/K,----------Vos=10uV、Ib=0.5nA,uVpp=0.23uV,这运放噪音低、精度高,Ib也不大,是7转10的首选。 
OP97F,较新的运放,Vos=30uV、Ib=0.03nA,uVpp=0.5uV,这运放尽管噪音稍大一点、但Ib很小,用做7转10的也很好,可以采用较大的比例电阻,732B里面就用这运放。 
OP297A,更新,性能比OP97F更好一点。 
以上运放,末位都带个7,可以认为都是以OP07为基础的改进型。 

LT1012C,Vos=10uV、Ib=0.03nA,uVpp=0.5uV。类似OP97F但Vos更小,适合7转10应用,只不过来源少、价格贵,金封更少见。 
OPA27,Vos=10uV、Ib=10nA,uVpp=0.08uV,这是低噪音高精度运放,Vpp不到1uV,当然,Ib比较大。 
OPA227,Vos=5uV、Ib=2.5nA,uVpp=0.09uV,改进的OP27,更高精度、更低的噪音,但Ib仍然偏大。 
LT1028,Vos=20uV、Ib=30nA、uVpp=0.035uV,显然,噪音非常非常小,只不过Vos不算最小的,尤其是Ib偏大。适合低内阻的微小电压放大。 

ICL7650S,Vos=0.7uV、Ib=4pA,uVpp=2.0uV 
这是老一些的斩波稳零运放,因此可以把Vos减到亚微伏级,同时Ib也很小,并可以基本消除1/f噪音,噪音指标从直流开始。当然,暫波稳零的运放噪音偏大一些,DC到10Hz的噪音有2.0uVpp,S7081里用了至少4片这运放,看来是在7转10、10转-10电路中用这做运放。 

LTC1052,Vos=0.5uV、Ib=1pA,uVpp=1.5uV 
这也是斩波稳零运放,同样Vos非常小、同时Ib也很小,也没有1/f噪音,DC到10Hz的噪音为1.5uVpp,这比7650稍微小了些。但在更低的频率DC-1Hz下,噪音有很大减少,为0.5uVp-p,这样就更适合直流。此运放在基准仪器里用的比较广,例如4910里用了至少6个(每路10V一个,4线10V用了2个)。

甚至3458A的ADC板内,其7转+12、+12转-12等所用的1825-1382,也怀疑是这个运放。 (补充:后来查明,这个运放是LT1001A,0.3uVpp噪音的高精度运放,Ib也不大,适合7转10之类放大)

AD8628,Vos=1uV、Ib=30pA,uVpp=0.5uV 
自称利用了斩波稳零和斩波技术,在保持低Vos和低Ib的同时,把0.1Hz到10Hz的噪音降低到0.5uVpp,而0.1Hz到1Hz的噪音为0.16uVpp。 
尽管指标,不是从DC开始的,DC到0.1Hz,从图上开噪音还是比较大,但也小于其它的自稳零技术的运放,作为低噪音电平转换是非常合适的。唯一一个小问题,就是供电电压最高只有5V,这样在7转10V的电路里,就需要采取措施把负供电提高上去(比如串联一个稳压管)。 

ADA4528-1,Vos=0.3uV、Ib=220pA,uVpp=0.1uV
这是较新的斩波稳零运放,尽管Ib大了一些,但低频噪音控制在惊人的0.1uVpp以下,这样就成为很理想的低噪声高精度放大的首选。当然,供电电压仍然只有5.5V最高。另外,封装很小,贴片MSOP,方形边长3mm,脚距为0.65mm,DIY的时候焊接比较费事,只能用转换插座。

转自:lymex

欢迎补充新元器件!!!