Other Parts Discussed in Thread: ADS1274, ADS1278, THS4521
设计TH4521+ADS1274的结构时,1274的VCOM输出2.5V,4521供电+5V 0V,看手册的意思好像放大器的输入在-0.2~2V,想问一下能否接双极性的输入信号?如果不行可以怎么做?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
-0.2~2V的输入共模电压范围是3.3V单电源供电,如果5V的话,输入共模电压范围为-0.2V~3.7V,低于-0.2V或者3.7V~5V之间的信号是不能处理的,所以如果需要接入双极性信号,建议双电源供电。Chao Meng 说:设计TH4521+ADS1274的结构时,1274的VCOM输出2.5V,4521供电+5V 0V,看手册的意思好像放大器的输入在-0.2~2V,想问一下能否接双极性的输入信号?如果不行可以怎么做?
非常感谢您的答复。现在我还有个疑问,在ADS1278的手册上表明 AINP-AINN在-VREF~+VREF之间,我的理解是:在1278的AVDD给5V,AGND给0V,VREFP给2.5V,VREFN给0V的情况下,模拟输入可以是双极性的,只要幅度在2.5V以下。而对于配套的TH4521输入则严格区分输入的正负,使得INP-INN必须在-0.2V~3.7V。这样的话,如果板子不能提供正负双电源,加上4521则不能检测双极性信号,而不使用4521直接接1278输入却可以。请问这样理解正确吗?
Vocm是为THS4521的输出设置的共模电压。与后面的ADC的输入共模电压相匹配。Chao Meng 说:还想问下4521中VOCM管脚输入的作用,是为放大器的输入提供偏置吗?由1278给出2.5V的VCOM接到4521的VOCM,是否输入就可以是双极性了?手册上写的还是不理解