我有一个电路是要FPGA输出一个脉冲,通过驱动电路驱动激光二极管输出脉冲光,所需驱动电流约750mA左右
脉冲的高电平在10ns左右,脉冲的频率不大(KHZ级别的)
请问TI有没有合适的驱动芯片方案?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最简单的方法:加入BUF634并联跟随 或者 多片THS3092并联
三极管嘛,3906和3904就好了
不过你方法好像错了;一般LD不用运放的;
比如激光测距:会选双栅极的MOS或者电容放电法