Other Parts Discussed in Thread: LMP91000
TI的工程师们,你们好,在使用LMP91000的时候,RE与CE短接,WE与CE之间输出几十豪伏,我在配置的时候Rload=100 ohm, Rtia=2.75K ohm, ZERO_INT=67%,Vias=10%,VER 使用外接基准2.5V,这时候量得到Vwe=1.438V,Vre=1.422V,Vout=1.838伏,这是怎么算得出来的呢?我根据框图算算不出这个值 来,麻烦指导一下。谢谢!
另外 ,当我拿开氧气传感器的时候,输出偏置是1.675V,2.5*67%=1.675V这跟配置符合,说明通信是没有问题的,并且我写完寄储器后还读出来,核对都是一样的。
I2c1_Write_Byte(LPM_ADDRESS,REG_LPM_LOCK,0);
I2c1_Write_Byte(LPM_ADDRESS,REG_LPM_TIACN,0x07);
I2c1_Write_Byte(LPM_ADDRESS,REG_LPM_REFCN,0xD6);
I2c1_Write_Byte(LPM_ADDRESS,REG_LPM_MODECN,0x03);
I2c1_Write_Byte(LPM_ADDRESS,REG_LPM_LOCK,0x01);