Other Parts Discussed in Thread: CD4052B
数据手册中。有提示电压VDD-VEE=20V的最大电压。但是实际使用时,CD4052B使用正负8V供电,IC就不能正常工作,降为正负6负就可以,但是系统为正负8负供电,另外稳压不方便。。。不知这个型号能不能这样供电,,,有没有其他代替的型号
VSS接的是GND还是其他电压?当VDD-VEE>13V的时候,VDD-VSS需要>4.5V 才可以。
if VDD – VSS = 3 V, a VDD – VEE of up to 13 V can be controlled; for VDD – VEE level differences above 13 V, a VDD – VSS of at least 4.5 V is required。