我的板子上GVDD,PVDD都是TPS5430产生的,DRV8412 的PVDD我用过5V,12V的,目前产品上电机时2.1V的,所以我把,对应的DCDC调到了2.5V,结果发现如果GVDD不接上12V,PVDD的电压是2.5V,如果GVDD给了12V,PVDD电压会上升到4V左右,应该是GVDD不知道为什么串到PVDD上了。
反复测试了好几个板子,最后的结论就是在PVDD小于5V的时候,GVDD不知道为什么串到PVDD上。
在PVDD是5V的时候,这些问题都没有。我查手册,也没发现DRV8412的PVDD和GVDD之间的压差有什么要求。请问为什么?谢谢