Other Parts Discussed in Thread: AFE4400
我有一个设计上用到两块AFE4400芯片,想把这两片芯片挂在同一个SPI口上与MCU通信。对于多设备连在同一个SPI上,手册上有如下描述:
“Note that when the AFE4400 is deselected, the SPISOMI, CLKOUT, ADC_RDY,PD_ALM, LED_ALM, and DIAG_END digital output pins do not enter a 3-state mode. This condition, therefore, must be taken into account when connecting multiple devices to the SPI port and for power-management considerations. In order to avoid loading the SPI bus when multiple devices are connected, the DIGOUT_TRISTATE register bit must be to 1 whenever the AFE SPI is inactive. ”
这段话的意思是,默认情况下,当一个SPI设备片选没有被选中时SPISOMI引脚不是高阻态,这导致没办法通信。手册提到的解决办法是在SPI没有被激活(inactive)时往DIGOUT_TRISTATE这个寄存器位上写1。有如下疑问:
(1)SPI没有被激活(inactive)是什么意思?因为任何对AFE4400的寄存器操作都要通过SPI,如果SPI没有被激活,如何进行SPI通信?
(2)SPISOMI引脚对于AFE4400是输出引脚,如果在复位后初始情况下(DIGOUT_TRISTATE为0),仅有一个AFE4400的spi片选被选中,这时两个AFE4400的SPISOMI是接在一起的,当输出不同电平时将会有冲突,如何解决?
能否提供一个多个AFE400接在同一个SPI总线的使用案例作为参考?
期望有人回答疑问,谢谢!