IWR1642BOOST二次开发的问题

Other Parts Discussed in Thread: IWR1642BOOST, UNIFLASH

1.现在使用的是IWR1642BOOST,默认配置了一根USB线,连接至PC,可以得到两个COM口。由于我们的工程需求,希望附加蓝牙或wifi模块,用蓝牙或者wifi的形式实现boost与PC之间的双向通讯,但是昨天尝试了一下,并没能实现通讯,希望您能给我一些建议,关于如何将板子与PC之间的通讯无线化。
2.将demo下载到ccs之后会出现dss和mss结尾的工程文件,我想问一下这两种工程具体是什么用途?在什么情况下需要对其进行修改?
3.拿到demo之后,如何进行二次开发?从哪里入手?有没有相关的开发案例?

希望各位技术大牛能够为我解答一下困惑。

  • 你好,
    首先是串口导出数据问题
    On the EVM, TM4C is a on-board XDS110 emulator.
    If you don't want to put a XDS110 on your board, you can use external USB<->UART cable to connect your board and PC.
    For mmwave demo, 2 UART is required for data and configuration transmit.
    Application/User Uart: Configuration port 115200bps: UART_RX/TX port <-> USB-UART cable <-> PC
    Auxilliary Data Port: Data port 921600bps: MSS_LOGGER-> USB-UART cable -> PC

    For flash the device using external USB<->UART cable:
    Set the SOP first, connect UART_RX/TX port <-> USB-UART cable <-> PC, then you can use uniflash to flash the device.

    If you have any further questions, please let me know, thanks.

    其实是DSS与MSS问题,
    DSS是C674 DSP的运行代码,mss是R4F MCU的运行代码。

    二次开发可以先看一下TI 提供的DEMO代码。文档位置
    file:///C:/ti/mmwave_sdk_02_00_00_04/packages/ti/demo/xwr16xx/mmw/docs/doxygen/html/index.html

    谢谢。
  • 您好,感谢您的回答!针对第一个问题,我想再请教一下,您这里说到如果不使用XDS110,使用两根USB-UART cable可以实现,我有两个问题:1. 是不是直接找到UART_RX/TX port和MSS_LOGGER这两个接口,用两根USB-UART cable连上,并各自与PC相连,就实现了同等的通讯功能? 2. 在1.的基础上,PC上显示出的COM口是不基于XDS110的,那么是不是需要提前对demo的上位机串口通信部分的内部进行修改,取消原有的只选取XDS110端口的限制? 3. UART_RX/TX port和MSS_LOGGER这两个接口在什么位置,在哪里可以查到相关的资料?
  • 你好,
    1 是的
    2 DEMO GUI不仅仅限制使用XDS110的串口?他应该可以识别所有串口吧?
    3. 接口在EVM上的两个connector上,请查看EVM原理图www.ti.com/.../sprr251

    谢谢。

    Regards,
    Wesley