XTR300输出不正常

Other Parts Discussed in Thread: XTR300, DAC8563

按照官方提供的原理图(DAC8563+XT300tidrhy3.PDF)做了4层版的DAC8563+XTR300双通道输出,元件参数与官方原理图一样。                                                        参考电压2.5V,设置为电压输出模式时,其中一个通道虽然输出电压可随输入在-5V-5V之间变化,但会产生振荡,输出波形有明                                                            显的杂波,去掉C26时就正常了。 而另一个通道始终输出+12V电压(我的电路是正负12V供电),用示波器测量5脚IMON,是一                                                          个振荡波形,正常的那个通道则是一个直流电压,测量4脚set端时电压为-8V左右,正常通道为0V左右。RG1和RG2连接的电阻调整                                                       也不起作用。测试了两块样板都是同样的问题,基本上可排除XTR300损坏,请问可能是什么原因导致了另一个通道的问题呢?