Other Parts Discussed in Thread: AM26LS31, THS4151, THS4150
有电机输出24V信号,为减少干扰,想转换为差分信号传输使用。有没有可以接受24V的单端转差分的芯片。
还有一种方案,之前有做过5V转换的,用的AM26Ls31,现在想,利用光耦将24V转为5V,经过AM26LS31转换差分,后端再用光耦将5V差分信号转为24V。(比较麻烦,光耦数量较多),如果采用此方案,请推荐光耦。
还有更好的方案也请推荐
后端差分输入要求什么幅值范围的?目前全差分运放的供电电压最大为33V,THS4150,THS4151等所以您现在是0~24V输出?最大33V电压的话,这样的话差分输出的其中一端肯定是饱和的,所以确认下接收端差分输入范围是多少?