问下我们现在生产通过吹气或加湿器加湿HDC1080传感器出现湿度值不升反降,会不会是热风回流焊造成的不良,用热风回流焊会有什么问题呢,为何要用红外回流焊呢?
您好,可以检查一下焊接是否符合手册第9.3.1节的描述:
When soldering the HDC1080 use the standard soldering profile IPC/JEDEC J-STD-020 with peak temperatures of 260 °C. When soldering the HDC1080 it is mandatory to use no-clean solder paste and no board wash should be applied. The HDC1080 should be limited to a single IR reflow and no rework is recommended