Other Parts Discussed in Thread: DRV5011, DRV5032, DRV5012
有一个产品需求如下:产品结构封闭,使用纽扣电池供电。产品生产完成后长期贮存(1年以上)。当需要使用时,需用外部磁场激活。现在考虑使用DRV5011或类似锁存型霍尔传感器,其输出开闭整个电路的供电。因为贮存时间内需要尽可能低的电流消耗。
看到DRV5011的ICC电流约为2.3mA左右,纽扣电池容量约100mAh左右,显然消耗太大。现在不理解该ICC参数。看到DRV5032的ICC电流在微安级别。
咨询DRV5011的ICC电流如何理解?是在不外加磁场的情况下的静态电流,还是磁场超过过BRP或者BOP之后的工作电流?
如果DRV5011不能满足这种需求,是否有其他方案推荐?