Other Parts Discussed in Thread: FDC2212, FDC2214
准备用FDC2212做踢脚开门,研究了一下,发现几个问题:
一、驱动电流如何转换成振荡幅度?
对应的寄存器地址:0x1E,0x1F
16uA~1.571mA-->1.2V~1.8V
二、规格书中的实例用什么参数计算的,怎么得出的7.5?
The SETTLECOUNT for any channel x must satisfy:
CHx_SETTLECOUNT > Vpk × fREFx × C × π2 / (32 × IDRIVEX) → 7.5, rounded up to 8. To provide margin
to account for system tolerances, a higher value of 10 is chosen.
三、应用INTB pin中断检测如何处理?
相关寄存器设置:DRDY=1,DRDY_2INT=1,INTB_DIS=0
那么INTB pin的状态是如何变化的?
四、检测天线有什么要求,连接INxA和INxB有什么区别?