Other Parts Discussed in Thread: TRF7970A
Dears:
我之前已经在官网上找过DATASHEET和代码来阅读了,手册里面说NFC的工作模式有点对点模式、读卡器模式、卡仿真模式、直接模式0、直接模式1,但是我不确定哪个模式比较适合我前面说的我们的应用场景,是不是用直接模式0比较合适?我们只是用NFC来传输一下蓝牙地址,数据量不大,十几二十个左右字节,这样是不是就不需要用到DATASHEET里面说的ISO14443a、ISO14443b、ISO15693、FeliCa这些协议?而是可以使用直接模式0,MCU通过NFC芯片的MOD引脚发送一段脉冲,然后可以在接收端的NFC的I/O_6(引脚 23)上,通过MCU去解析收到的脉冲来得到数据?官网上的代码我看过了,是带ISO14443a、ISO14443b、ISO15693、FeliCa这些协议的,没有直接模式0的demo代码