Other Parts Discussed in Thread: TS5A6542, SN74ALVC164245
您好,
我有两个问题,第一个是关于TS5A6542的,具体电路见下图
VCC_CTRL_1是通过FPGA产生的控制信号(0V OR 3.3V),经过SN74ALVC164245芯片调理后,变成0V OR 5.0V,这个电路的目的是通过调节VCC_CTRL_1,选择VCC_SUPPLY,可是,当VCC_CTRL_1不管是L还是H,输出的电压幅值均为1V左右,这是为什么?
第二个问题是:我使用1N4148组成如下图电路,为什么当我不接R2或者R2不为0时,可以输出我想要的波形,可是当R2为0时,为什么输出的波形是一条直线,为0呢?输入幅值0~5V,输入频率50HZ?