Other Parts Discussed in Thread: TMP102
我们公司目前使用TI的温度传感器TMP102近500个,用于测量溶液温度,溶液主要是弱酸弱碱类,温度37℃左右;
每根贴片的PCB温度探头都会先测试,然后封装到金属管内密封(TMP102电路板和金属管之间填充的导热硅胶)再次测试并标定,测试和安装过程中没有发现不良品。但是在成品使用中,到目前共发现有5个坏掉的,坏掉的温度传感器平均使用时间2-3周内。出现了几种情况:1.IIC能通信,但始终为0;2.IIC能通信,但只能输出31.9℃、63.9℃、127.9℃;3.不通信或返回均为0xFFF。
分析结果大概是,第一种情况,SDA引脚与GND引脚之间阻值低于80,数据线被拉低,所以数据始终为0。
TMP102在什么情况下会出现这些问题;出厂时合格率是否100%;我们应该怎么测试才能够及早发现有异常的芯片(避免在用户那里出现问题);该芯片会受到哪些环境因素的影响而导致不稳定或损坏;