This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5731M 输出功率最小是多少?



您好!

目前我们项目使用的5731M为2.1mode, 2*5W + 10W,Vcc:3.3V + 15V。

但是目前需要改为2.0mode , 2*2.5W。在不改变供电的情况下,是否可以实现这样的低功率输出呢?

如果采用SE,Channel C,D可能会闲置,这样是否会有问题呢?